Search

Start main contents

  • Register
  • Login

Solutions

Print page

Solutions

Safety

Devices and Components

Devices and Components

Networks

CC-Link Safety is an open communications network that is suitable for safety applications because it guarantees reliability in data transmission. It complies with IEC61508 SIL3 and EN954-1/ISO13849-1 Category 4 and is compatible with other CC-Link products. CC-Link Safety will detect communication failures such as unexpected delay of communication or erroneous data that may cause malfunction of the emergency stop operation. This fail-safe function will bring machinery into a safe condition quickly if a communication failure is detected.

Sensors

Mitsubishi Electric has a best in class strategy with regard to safety sensors that allows customers to select the products that optimize their application. From selecting e-stops to light curtains, Mitsubishi Electric provides the interfaces that enable connectivity to a broad range of safety sensor technologies.


Industry 4.0 White Paper – The fourth industrial revolution has created what has been dubbed ‘Industry 4.0’. This white paper explains the background, consider the challenges and offer solutions to the adoption of I4.0.
More
Page top