Search

Start main contents

  • Home
  • Next generations - Meet the demands of tomorrow
  • Register
  • Login

Factory Automation

Print page

Factory Automation

Next generations - Meet the demands of tomorrow

4 great new products designed to meet the demands of tomorrow! The successors to the compact MELSEC FX PLC series and the modular automation concept MELSEC iQ Platform, the brilliant HMI GOT2000 series and the FR-A800 high-end frequency inverter are waiting in the wings.

HMIs with multi-touch function and gesture control - GOT2000 series (available from March 2014)

Mitsubishi Electric has raised the bar for HMIs with the new GOT2000 series, designed to optimise operator control and monitoring of device and line status. With vastly increased performance, advanced functions, seamless connectivity to other automation devices and highly intuitive, tablet-like operation* and the highest quality graphics, the new GOT2000 series provides a range of models and sizes to meet the needs of the broadest spread of applications. With their enhanced functionality, these new HMIs extend capabilities beyond monitoring and visualisation, providing additional features that will help to reduce downtime, enable fast recovery from simple errors, increase availability and boost production efficiency.

More than simply displaying data, these enhanced HMIs deliver genuine perspective on the automation process and provide a platform to solve the typical production problems that drive down OEE.

A comprehensive line-up of products provides screen sizes from 8.4” up to 15” (to be expanded to include from 3.7” up to 19” in the future) in two basic ranges: the GT27 for high end applications that demand the highest levels of performance and functionality; and the GT23 for cost-sensitive applications that can now benefit from new benchmark performance standards. In addition, a software HMI version, the GT SoftGOT2000, realises all of the GOT2000 features on a PC or panel computer.

Features and benefits:

  • Benchmark performance
  • Increased memory size
  • Multi-touch/gestures*
  • Beautiful graphics
  • Advanced communications
  • Easy screen design
  • Backwards compatibility
  • Horizontal integration

* Some functions such as Multi-touch/gesture are only available on certain models

Download now

Maximum drive performance for plant and machinery – FR-A800 frequency inverter series (available from April 2014)

Designed for unparalleled drive precision, speed control, simple startup, and versatility, Mitsubishi Electric has developed a new generation of drive technology: the remarkable FR-A800. This new drive series is the successor of the highly successful FR-A700 series. It is equipped with the new state-of-the art high-speed processor by Mitsubishi Electric. With better than ever control performance and response level, safe and accurate operation is assured in a diverse range of applications. Some of the outstanding features are the integrated USB port for programming and parameter copying, an-easy to-read control panel, optimum power usage and energy saving functions, improved system safety, three expansion slots for a range of option and supported network cards.

With it’s impressive versatility to meet equipment system needs ranging from machining and molding to winding, the FR-A800 is a extremely economical and highly-versatile solution for a wide range of applications.

The FR-A800 series is fully backwards compatible with the FR-A700 series. Parameters can be easily copied by FR Configurator2. In order to match the former machine response time, the input/output signals of the FR-A800 can be delayed.

Features and benefits:

  • Real Sensorless Vector Control
  • Perfect autotuning of PM and IM motors
  • Absolute postioning & built-in PLC function
  • Optimum excitation control
  • High flexibilty by built-in PLC
  • Energy saving by 24 V control power supply
  • Improved system safey
  • Easy operation
Download now

The next generation iQ Platform – iQ-R (available from 3rd quarter 2014)

Mitsubishi Electric has launched its next generation CPU for the iQ Platform programmable automation controller (PAC). The new iQ-R series CPU offers dramatic improvements in performance, setting new benchmark standards for processing speed. This not only enables users to realise enhanced system designs, but also provides the basis for significant reduction in hardware costs. At the same time, the new iQ-R series offers reductions in development cost, maintenance cost and risk of system failure, while providing an innovative upgrade path that will enable users to take advantage of ongoing developments through software upgrades rather than hardware upgrades.

The iQ Platform builds on the power of Mitsubishi Electric’s high performance PACs, complementing this with a broad range of control modules and network interfaces. This adaptable and powerful control platform enables companies to take a strategic approach to automation and control, allowing full integration of the plant floor operations within the business functions.

Features and benefits:

  • High performance CPU
  • Synchronised control
  • Secure data storage
  • Reduced maintenance effort
  • Seamless device connectivity
  • Efficient engineering – GX Works3
  • System security
  • MELSEC System Q compatibility
Download now

“All-inclusive standard” in the field of compact controllers - MELSEC FX5 (availabe from 3rd quarter 2014)

With the launch of the FX5 compact PLC, Mitsubishi Electric has made the world’s best selling PLC even better. Since the launch of the original FX over 30 years ago, Mitsubishi Electric has sold over 13 million units across the globe. As the first compact PLC to be seen in the European market, the FX transformed automation by bringing PLC control and functionality into smaller, lower cost applications that would previously have had to rely solely on discrete relay-based logic. For over three decades, Mitsubishi Electric has been the market leader in this sector. Now, with the introduction of the new FX5, Mitsubishi Electric has given these compact controllers a huge performance boost, focusing on processing power, expansion, built-in functionality and positioning & motion functions.

At the same time, users benefit from simpler programming and reduced maintenance effort to greatly reduce the total cost of ownership.

Features and benefits:

  • Superior performance
  • High speed input & outputs
  • Built-in analogue and PID control
  • Built in Ethernet
  • Advance positioning & motion functions
  • CC-Link IE Field interface
  • Improved connectivity
  • Low total cost of ownership
  • Advanced troubleshooting
Download now


Back

Page top